Center Frequency

Sets the frequency that corresponds to the horizontal center of the graticule (when frequency Scale Type is set to linear). While adjusting Center Frequency, Span is held constant, which means that both Start Freq and Stop Freq will change.

Pressing Center Frequency sets the frequency entry mode to Center/Span. In Center/Span mode, the center frequency and span values are displayed below the graticule, and the default active function in the Frequency menu is Center Frequency. In the Start/Stop annotation mode, Start Freq and Stop Freq are displayed below the graticule instead of Center Frequency and Span.

Pressing Center Frequency also sets the frequency entry mode to Center/Span. In Center/Span mode, the center frequency and span values are displayed below the graticule, and the default active function in the Frequency menu is Center Frequency.

When Display Scale Type is set to LOG, pressing Center Frequency sets the frequency that corresponds to the arithmetic mean of the start frequency and stop frequency, which is not at the horizontal center of the graticule.

The center frequency setting is the same for all measurements within a Mode, that is, it is Meas Global. Some Modes are also able to share a Mode Global center frequency value. If this is the case, the Mode has a Global tab in its Meas Setup menu.

Center Frequency sets (and queries) the center frequency for the currently selected input. If your instrument has multiple inputs, and you select another input, Center Frequency changes to the value for that input. SCPI commands are available to directly set Center Frequency for a specific input (see RF Center Frequency and Ext Mix Center Freq).

Center Frequency is remembered as you go from input to input. Thus, you can set a Center Frequency of 10 GHz with the RF Input selected, change to BBIQ and set a Center Frequency of 20 MHz, then switch to External Mixing and set a Center Frequency of 60 GHz. When you return to the RF Input, Center Frequency reverts to 10 GHz; back to BBIQ and it is 20 MHz; back to External Mixing and it is 60 GHz.

Remote Command

[:SENSe]:FREQuency:CENTer <freq>

[:SENSe]:FREQuency:CENTer?

Example

Set Center Frequency to 50 MHz:

:FREQ:CENT 50 MHz

Increment Center Frequency by the value of CF Step:

:FREQ:CENT UP

Return the current value of Center Frequency:

:FREQ:CENT?

Notes

Sets the RF, External Mixing or I/Q Center Frequency depending on the selected input:

  • For RF input it is equivalent to :FREQ:RF:CENT

  • For I/Q input it is equivalent to :FREQ:IQ:CENT

  • For External Mixer it is equivalent to :FREQ:EMIX:CENT

Preset and Max values depend on Hardware Options

If no terminator (for example, MHz) is sent, the terminator Hz is used. If a terminator with unit other than frequency is used, an invalid suffix error message is generated

Dependencies

Center Frequency can be limited by Start Freq or Stop Freq limits, if Span is so large that start or stop reach their limits

Couplings

When operating in “swept span”, any value of Center Frequency or Span that is within the frequency range of the instrument is allowed, if the value is being set through the front panel numeric key pad or the SCPI command. The other parameter is forced to a different value if needed, to keep Start and Stop Frequencies within the instrument’s frequency range

Coupling between center frequency and span: numeric (keypad) entries are treated differently than changing the value using the step keys (Up/Down Arrows) or the knob. Similarly, for remote operation, sending a numeric frequency value is treated differently than the UP|DOWN keywords:

  • Numeric entries (keypad or remote): Any value of Center Frequency or Span (within the frequency range of the instrument) is allowed. The other parameter is changed, as necessary, to keep the Start Freq and Stop Freq within the instrument frequency range

  • Knob or Step keys (up/down arrows) or UP|DOWN keywords: The value of the parameter being changed (Center Frequency or Span) is limited so the other parameter is not forced to a new value. Thus, if only the step keys and knob are used, you can return to the initial Center Frequency and Span by changing only the current parameter

Note that, since out-of-range Start Freq and Stop Freq are never allowed, markers and trace math work correctly without requiring any special handling for out-of-range conditions

Preset

Depends on instrument maximum frequency, mode, measurement, and selected input

See Center Frequency Presets and Ext Mix Center Freq

State Saved

Saved in instrument state

Min/Max

Depends on instrument maximum frequency, mode, measurement, and selected input

See Center Frequency Presets and Ext Mix Center Freq

Annotation

Center <value> appears in the lower left corner of the display

Status Bits/OPC dependencies

Non-overlapped

VXT Models with Radio Heads/CIU Frequency Range

The following table shows the Center Frequency Presets and Range for VXT modes with Radio Heads/CIU.

Products with Radio Heads/CIU

Preset

Start frequency

Stop frequency

M9421A + CIU

6 GHz

5.9 GHz

12 GHz

M9410A + CIU

6 GHz

5.9 GHz

12 GHz

M9410A + CIU + RRH

25 GHz

24.25 GHz

43.5 GHz